Toolbars

Window Control Toolbar

The Window controls are located along the top of the main window.

From left to right:

Open files.

Controls traces on the display.

Opens Help files.

Accesses offline traces.

Exports display data.

Graph Toolbar

The Graph toolbar is located directly below the displays. Use the toolbar to control the display.

From left to right:

Flag - Indicates an annotation at a specific location (time) on the graph.
Diamond - indicates the location of a vertical marker.
Left arrows - autoscrolls to the left of the graph.
Four arrows - autoscales vertically and horizontally.
Vertical arrows - autoscales vertically.
Horizontal arrows - autoscales horizontally.
Area plus - zooms in by region.
Plus - zooms in
Minus - zooms out
Graph gear - displays the trace configuration selections

The ARB Toolbar

The ARB toolbar is located directly below the display. Use the toolbar to edit the trace sequence.   

From left to right:

- Undoes the previous action.
- Redoes the previous action.
Move Left - moves the highlighted waveform one position left.
Move Right - moves the highlighted waveform one position right.
Insert Left - inserts a new waveform space to the left of the selected waveform.
Insert Right - inserts a new waveform space to the right of the selected waveform.

Clone - clones the highlighted waveform and insert the clone to the right of the waveform.

Delete - deletes the highlighted trace.

Trace - lets you save an ARB trace to a file.

Clear - Current clears all current traces.

Clone Traces - clones the selected trace to another output channel or to the alternate function (either voltage or current) on the same output channel. Click and drag the trace to the desired location. Note that if you copy a voltage trace to a current trace on the same output, the voltage trace will be removed. This is because you cannot generate both a voltage and a current trace on the same output